Video/Written Case Studies


Sunoco Case Study
Along with several refineries and chemical plants, as well as thousands of miles of pipeline, Sunoco boasts over 5,000 convenience stores and service stations. When Sunoco was looking for a way to monitor these locations, they turned to Interface and Honeywell. Interface installed a state-of-the-art digital solution that included a central monitoring facility that enabled Sunoco to monitor events at all their locations.
  View the PDF       View the Video
 
Land Tejas Case Study
Land Tejas in Houston, TX has a primary focus to develop master planned communities that incorporate technology. After checking the capabilities of various manufacturers, they selected Honeywell to provide home automation, security and structured wiring. Since energy management was important to Land Tejas, they also used Honeywell’s Internet Connection Module so that the thermostats and security system could be integrated, allowing the security system to tell the thermostat whether the homeowners where home or away, which results in energy savings.
  View the PDF        View the Video
 
St. Georges Technical High School
St. Georges Technical SchoolSt. Georges Technical High School in Middletown, DE turned to security integrator Advantech and Honeywell to provide an integrated security management system. Advantech installed a one system/one card solution with true data integration of the sub-systems, including IP video, intrusion and smart card technology.
  View the PDF        View the Video
 
Cox Enterprises, Inc.
Cox Enterprises, Inc.Cox Enterprises, Inc. of Atlanta, Georgia has grown to be one of the nation’s premier media companies and providers of automotive services.  On a daily basis, anywhere from 2500 to 3000 people move through the corporate headquarters. Cox was looking for an automated badging control system to provide an increased level of security to protect their greatest asset: their employees. They selected security integrator Security 101 and its partner of choice Honeywell to provide the solution.
  View the Video
 
SunRiver Development Selects Honeywell
SunRiverBuilder/developer Darcy Stewart had a vision to create an active adult lifestyle community using the latest home automation technology throughout the development and inside the homes.
  View the PDF          View the Video
 
Port of Wilmington
Port of WilmingtonThe Port of Wilmington is the largest container port on the Delaware River. Honeywell worked with security integrator Advantech to design an access/cctv/intrusion detection system to cover both land and water perimeters.
  View the PDF          View the Video
For a copy of the DVD, call 1-800-796-2288, option 3 and ask for L/PORTDVD/D.
 
Morristown Municipal Airport
Conducting more than 220,000 operations a year, Morristown Airport is a general aviation reliever airport in the New York metropolitan area. The Airport contracted security integrator Service Works, Inc. (SWI) who created a Honeywell solution that includes IP-based video, as well as card access control.
  View the PDF          View the Video
For a copy of the DVD, call 1-800-796-2288, option 3 and  ask for L/SWIMADVD/D.
 
Delaware State University
Advantech selected Honeywell’s ProWatch Security Management System, a multi-tiered client server architecture, as a multi-campus solution for integration of DSU’s building and vehicle access control, CCTV, ID badging, intrusion detection, asset detection, and fire alarm systems.
  View the PDF          View the Video
For a copy of the DVD, call 1-800-796-2288, option 3 and  ask for K14147.
 
The Peninsula
The PeninsulaThe Peninsula is a world-class resort community that includes town homes, villa homes, custom homes and condominiums. Advantech designed a comprehensive security management system for this gated community using Honeywell technologies, which include Pro-Watch and Lobbyworks, a web-based visitor management system.
  View the PDF          View the Video
 
Central Valley Community Bank
Central Valley Community BankMatson Alarm Company used a variety of Honeywell technologies to protect the employees and customers at Central Valley Community Bank. A highlight of the installation was Honeywell’s new GSM radio product that offers the bank additional security. Also included in the installation were a variety of cameras to protect the ATM, teller cages and exterior of the building. The bank believes the Honeywell technologies were a great improvement since the system was easy to use, the pictures were clear and easy to share with law enforcement in an emergency.
  View the PDF     View the Video
 
RFK Stadium
A 56,000-seat stadium, the RFK Stadium in Washington, D.C. is home to Major League Baseball’s Washington Nationals and Major League Soccer’s DC United. The stadium’s management company selected ASG Security to upgrade the existing system before the inaugural season of the new Washington Nationals baseball team. ASG installed a Honeywell video security system that consisted of 56 cameras, rugged housings and lenses, a MAX-1000 switcher, three Fusion DVRs and the ULTRAKey system.
  View the PDF          View the Video
 
Search

Be Considered for a Partner of Choice profile

If you would like to be considered for a case study, click here.