|
System Is Industry’s First to Offer Video Without the Need for DVRs or NVRs
LOUISVILLE, KY, June 26, 2012 – Honeywell (NYSE: HON) has added advanced video capabilities to one of its most-popular – and most-affordable – access control systems, giving owners of small to mid-size businesses a new option for improving building security. The company’s award-winning NetAXS-123 offering is the first access control technology of its kind to provide video surveillance without requiring a digital video recorder (DVR) or network video recorder (NVR), making it ideal for smaller businesses such as restaurants, convenience stores, medical clinics and health clubs.
Instead of DVRs or NVRs, the system allows businesses to store video on USB memory sticks. And while most video systems record continuously, NetAXS-123’s video capabilities offer event-based recording, meaning users can set the system to record only certain access-control events such as a door being propped or forced open, or someone trying to enter the premises using an invalid card. The technology significantly reduces the amount of time and effort needed to set up the overall system with its ability to automatically discover cameras connected to it, as well as intuitive, easy-to-use set-up screens.
“Smaller businesses need effective security just as much as large corporations, but they have far fewer resources to work with, and many times they simply can’t afford an elaborate security system,” said Erica Morris, senior customer marketing manager for Honeywell. “These smaller businesses and organizations shouldn’t have to sacrifice protection, and NetAXS-123’s new video capabilities provide the type of security you would have at larger complexes, but at a much lower total cost of ownership.”
NetAXS-123 is a web-based access control system designed to protect facilities with fewer than three doors. The panel uses built-in Ethernet and USB support, as well as Power over Ethernet (PoE) capability to reduce installation costs and eliminate the need for wire runs to power the unit. Its compact, modular design allows businesses to purchase the right amount of access control they initially need, and also quickly and easily expand as those needs change. The new Video Add-On Kit lets customers use live video to monitor their sites remotely and visually confirm access control events.
The system’s simplified installation and user training, as well as the minimal post-sale support required, make it ideal for security dealers who want to expand their businesses with access control technology. It will be available for a live demonstration at the Electronic Security Expo (ESX) in Nashville on June 27-28.
For more information, please visit
www.honeywellaccess.com/netaxs123.
Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.
This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.
|