Honeywell

CONTACT & SUPPORT  |  WORLDWIDE  Worldwide Locations    

 Search
Press Releases
  Back
Sep 04, 2012
Honeywell Unveils Compact, High Security Seismic Vibration Sensor

Versatile New SC100 Series Delivers Robust Protection for ATMs, Safes and Vaults; Offers Easy Installation and Reduced Costs

MELVILLE, N.Y., September 4, 2012– Honeywell (NYSE: HON) today announced the release of the SC100 Series Seismic Vibration Sensors designed for the protection of high-value assets in financial, retail and other applications. The series includes two compact, high security sensors: the SC100 and the SC105. The SC100 detects heat and vibrations resulting from attempts to disturb solid structures including fixed ATMs, bank vaults, safes, ATMs and doors. The SC105 is equipped to safeguard freestanding objects like mini ATMs, gun cases, vending and ticket machines or to secure file cabinets in noisy environments. Both models can be installed in new or existing security systems and offer a higher level of protection over traditional shock sensors, which often lack the ability to discriminate between ambient vibration and real attacks.

Advanced sensing technology reduces the potential for false alarms while detecting heavy strokes from sledgehammers, repeated knocks from hammer and chisel attacks, drilling, mechanical cutting, acetylene torches, diamond drills, hydraulic jacks and more. The compact size enables placement inside small hardware—letting security dealers safeguard items that were previously difficult to protect.

Installation is simple, with built-in end-of-line (EOL) resistors that improve connectivity to the control panel—boosting reliability and reducing service calls and associated costs. In addition, the products contain an integrated temperature alert feature—eliminating the need for additional sensors and, in turn, reducing dealer inventories and related costs.

For more information, please call 1-800-467-5875.


Honeywell (www.honeywell.com) is a Fortune 100 diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; turbochargers; and performance materials. Based in Morris Township, N.J., Honeywell's shares are traded on the New York, London, and Chicago Stock Exchanges. For more news and information on Honeywell, please visit www.honeywellnow.com.


This release contains "forward-looking statements" within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of fact, that address activities, events or developments that we or our management intend, expect, project, believe or anticipate will or may occur in the future are forward-looking statements. Forward-looking statements are based on management's assumptions and assessments in light of past experience and trends, current conditions, expected future developments and other relevant factors. They are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by our forward-looking statements. Our forward-looking statements are also subject to risks and uncertainties, which can affect our performance in both the near- and long-term. We identify the principal risks and uncertainties that affect our performance in our Form 10-K and other filings with the Securities and Exchange Commission.

Contact:
Ralph Maniscalco
Honeywell
516-577-2803
ralph.maniscalco@honeywell.com



  Back Back to top   


 

SITEMAP