Caught on Tape: Iowa School District Uses Digital Video Technology to
Curb Stop-Arm Violations
School buses are the safest vehicles on the road – 70 times safer than cars,
light trucks and vans. Yet an average of 33 school-aged children are killed each
year in bus-related accidents in the United States; the majority of those deaths
occur in the “danger zone,” the 10-foot area surrounding the bus, because of
passing motorists who disregard a bus’ stop arm.
Spencer Community School District, located in northwestern Iowa and serving
more than 2,400 students, is one of the fortunate districts – not a single
fatality has been recorded despite the dozens of motorists who made a habit of
illegally passing school buses. The district’s transportation supervisor, Dan
Schultz, intends it to stay that way.
Schultz heard the bus drivers’ complaints of passing motorists, but didn’t
know how to prove these violations were occurring. He knew there must be a
solution and began researching video technology that would record stop-arm
violations – irrefutable evidence of breaking the law.
Schultz was especially concerned about stop-arm violations occurring around
the bus that carried Spencer’s 3- and 4-year-old vulnerable pre-schoolers. With
the blessing of the Iowa Pupil Transportation Association (IPTA), the Iowa
Department of Education purchased one VHS-based analog video recording system
for Schultz to use on the pre-school bus. The camera was mounted on the inside
of the bus facing outward, and recorded drivers who passed illegally.
When a stop-arm violation occurred, bus drivers would say the car’s license
plate number out loud, describe the vehicle and make note of any witnesses, all
of which was recorded through the system’s audio input. The driver would then
report the violation to Schultz, who filled out an incident report. Schultz then
turned the case and the video over to the police, to further investigate the
violation and identify the offender.
In a six-month trial period with one camera installed on the pre-school bus,
40 drivers were caught and all but three pleaded guilty after viewing the tape.
The local newspaper and radio station reported on Spencer’s new recording
system, and drivers took notice.
In the second six-month recording period, only four drivers were caught
passing school buses.
Schultz credits the Spencer Police Department for being so cooperative and
accepting the additional investigation work on top of their regular
responsibilities.
“The Spencer police have become our partners,” Schultz said. “We tape the
violations, hand them to the police and they take care of the rest. We know they
are committed to student safety as much as we are.”
Schultz found that one of the major benefits to recording the stop-arm
violation was the tangible proof the tape offered. In all but a few instances,
drivers confessed immediately upon seeing the tape. Their early confessions
saved time and money by not going to court.
“It’s nearly impossible for drivers to talk their way out of a stop arm
violation," Schultz said. “We have it on tape – you can’t dispute video
evidence.”
In one instance, authorities discovered that one of the caught individuals
was not allowed to walk outside because of his medication, let alone drive a
car. Another individual, who had repeatedly gotten out of stop arm violations by
accusing the bus driver of entrapping his car, was finally found guilty after he
viewed the tape and confessed.
Though the VHS system had been successful at catching stop arm violators, its
image quality proved problematic at times, and without a date and time stamp,
Schultz and his drivers had to search through hours of footage to find the
passing motorist. The transportation department went through 40 videotapes in
six months – when a tape contained a suspected violation, it could not be
re-used until the trial date.
Schultz decided to upgrade and purchased a digital recording system: the
Digital Chaperone by Honeywell. It provides crisp, clear images, the ability to
e-mail photos to police and also to focus in on various points. The Digital
Chaperone also allows for multiple cameras to record continuously. Each bus has
three cameras: one camera faces forward, recording any stop-arm violations; and
two face backward, recording the students aboard the bus. Of the two cameras
facing backward, one is located near the rear and one near the front to record
the driver and student audio.
The digital system provides several additional benefits over the VHS-based
analog system. Schultz can access the video cameras at any time from his laptop
computer. Instead of scanning through hours of videotape, Schultz and his
drivers can pinpoint the incident. Images are recorded with the vehicle
identification, date, time, camera name, and various status inputs, which allows
for more accurate investigations. Honeywell’s system also comes with BusViewTM
software that allows Schultz to find, print, distribute and archive video and
audio files. Schultz has found the ability to e-mail images to police and school
administration among the most useful features of the digital system because it
speeds up the investigation process.
“Spencer’s administration has been extremely supportive of the new digital
system because they can actually see incidents occurring on tape when I e-mail
them the still photo or video,” Schultz said. “Seeing is believing, and they’re
glad to help remedy our passing motorist problems.”
Schultz also uses the system for bus driver evaluations, and credits it for
saving valuable time. He’s able to make sure bus drivers are following protocol
at railroads and intersections, information he may not be able to gather during
a supervised ride-along.
“I used to ride along with each bus driver as part of their review, which
took a total of 32 hours – almost an entire week’s worth of work,” Schultz said.
“Now I can pick random days to check in on each bus, which only takes 15 to 20
minutes per driver.”
The system also features triggers that monitor driver inputs, such as stop
arm use, brakes, speed, turning and warning lights. By reviewing the footage
around the specific incident, police can determine whether the driver was
performing correctly. If the stop arm was not deployed as it should have been,
the suspected stop-arm violator cannot be prosecuted.
Identifying bus stop and route improvements was an unexpected benefit of the
recording system, Schultz said. “After reviewing footage, I was able to make
recommendations for moving some bus stops farther from busy street corners,”
Schultz said. “This gives drivers more notice, so they’re more likely to stop an
appropriate distance behind the bus.”
Because of Spencer’s success using a digital video recording system, the Iowa
Pupil Transportation Association is in talks about expanding the program. The
goal is each school district will be able to have a similar video system. The
state currently owns eight systems – six VHS and two digital – that are shared
among districts who use them for the year. Schultz, who is also the president of
the IPTA, said that although the digital system is a pricier option, its
benefits far outweigh those of the analog system.
“With an analog system, you’re stuck with what you’ve got,” Schultz said.
“Digital systems allow you to expand and upgrade as your needs increase. Going
digital makes sense for the future.”
These days, things are quieter – less hurried – in Spencer. Schultz is proud
to say that the district has never had a two-time violator, and because of this,
he knows the system is working. While there were 40 violations in the first six
months of system use, there were only four the remainder of the year.
For school districts considering a stop-arm violation reduction program like
Spencer’s, Schultz recommends getting all parties on board before buying the
equipment to avoid any miscommunication or unrealistic expectations.
“Bring in the authorities before starting your program, and explain that you
want open lines of communication. Explain how the community benefits from a
program like this,” Schultz said. “The cornerstone of the project is still the
investigations into violations, so the police department must sign on for the
added responsibilities.”
Now, when Spencer replaces an older school bus, the new bus is outfitted with
a digital system. Schultz is excited that Iowa has been so receptive to video
recording systems, and would like to see a nationwide program where schools
could qualify for funds to outfit their entire bus fleet with digital systems.
“It’s not just about the safety of one child during one incident,” Schultz
said.
“It’s about protecting all of our students, and preserving the safety
of all children.” |