<< Back

Press Releases

 
 

Honeywell Introduces New ACUIX™ PTZ Cameras

High Speed Dome Cameras Save Time for Installers and End Users

RUNCORN, UK, April 28, 2008 – Honeywell (NYSE: HON) today introduced the new ACUIX™ series of high performance pan/tilt/zoom (PTZ) speed dome cameras that feature multiple housing configurations and four integrated high-resolution, auto-focus camera/optic systems. The series was created to consolidate the Honeywell PTZ dome camera line-up to a single platform, which will support both analogue and digital (IP) video transmissions.

ACUIX works seamlessly with all current and future Honeywell video and surveillance products. The series incorporates Honeywell’s proprietary Intellibus™ protocol for high-speed performance and effortless upgrades. Intellibus allows camera settings such as labels, presets, tours, and privacy zones to be uploaded to a new camera/optics package if required, affording the ultimate protection of the dome’s settings. Because Intellibus allows users to remotely upload firmware to a single dome - or an unlimited number of user-selected domes, ACUIX offers major time savings for dealers and end users.

“ACUIX incorporates innovative features such as remote storage of camera data and remote firmware upgrades. This allows installers to perform set-up and maintenance from their lab benches, which in turn minimises installation time at the customer site and eliminates complications at the top of a ladder,” said Mark Openshaw, product manager, Honeywell. “Customers and installers alike will appreciate the remarkable performance of ACUIX and its ease of use.”

The series includes a True Day/Night model with a 35X zoom featuring Wide Dynamic Range and Electronic Image Stabilisation for superior images that overcome unstable mounting and difficult lighting conditions. The ACUIX speed dome cameras provide intelligent vision for any indoor or outdoor surveillance applications. Its sharp images, high reliability and flexible mounting options make ACUIX ideally suited for retail stores, schools and campus environments, industrial sites, casinos and locations where traffic monitoring is essential.

For more information, visit www.honeywell.com/security/uk


Honeywell International is a $36 billion diversified technology and manufacturing leader, serving customers worldwide with aerospace products and services; control technologies for buildings, homes and industry; automotive products; turbochargers; and specialty materials. Based in Morris Township, N.J., Honeywell’s shares are traded on the New York, London and Chicago Stock Exchanges. For additional information, please visit www.honeywell.com.


This release contains certain statements that may be deemed “forward-looking statements” within the meaning of Section 21E of the Securities Exchange Act of 1934. All statements, other than statements of historical fact, that address activities, events or developments that we or our management intends, expects, projects, believes or anticipates will or may occur in the future are forward-looking statements. Such statements are based upon certain assumptions and assessments made by our management in light of their experience and their perception of historical trends, current conditions, expected future developments and other factors they believe to be appropriate. The forward-looking statements included in this release are also subject to a number of material risks and uncertainties, including but not limited to economic, competitive, governmental, and technological factors affecting our operations, markets, products, services and prices. Such forward-looking statements are not guarantees of future performance, and actual results, developments and business decisions may differ from those envisaged by such forward-looking statements.


 
Contact:
 
Sue Howes
Honeywell Access Systems
+44 7766 420250
sue.howes@honeywell.com

 
Guy McGerr
Weber Shandwick Technology
00 44 20 7067 0337
gmcgerr@webershandwick.com



 

 Back to top


Search